TYPE Visu_ClientType :
This enumeration is in fact the same than Visu_ClientTypeItf within VisuItfs. To prevent damaging installations of older versions where Visu_ClientType was already defined within VisuElemBase (-> Ambiguity), we must not move this enum to VisuItfs without renmaing it. As Visu_ClientType was part of the visualization elements interface and cannot be removed for that reason, we have those duplicates here! REMARK: When doing changes here, please adapt VisuItfs.Visu_ClientTypeItf accordingly too!!!
InOut: |
|