FUNCTION_BLOCK VisuFbFileTransferManager
Methods:
FB_Exit FB_Init GetParamForFileTransf GetParamForStreamTransf GetStringBuffer NormalizeFilePath RequestStreamingPlcToVisu RequestStreamingVisuToPlc RequestStreamingVisuToPlc2 RequestTransfer RequestTransfer2 RequestTransfer3 ClientRemoved ReadFileName
FB_Exit
FB_Init
GetParamForFileTransf
GetParamForStreamTransf
GetStringBuffer
NormalizeFilePath
RequestStreamingPlcToVisu
RequestStreamingVisuToPlc
RequestStreamingVisuToPlc2
RequestTransfer
RequestTransfer2
RequestTransfer3
ClientRemoved
ReadFileName
Structure:
FB_Exit (Method)
FB_Init (Method)
GetParamForFileTransf (Method)
GetParamForStreamTransf (Method)
GetStringBuffer (Method)
NormalizeFilePath (Method)
RequestStreamingPlcToVisu (Method)
RequestStreamingVisuToPlc (Method)
RequestStreamingVisuToPlc2 (Method)
RequestTransfer (Method)
RequestTransfer2 (Method)
RequestTransfer3 (Method)
internal
ClientRemoved (Method)
ReadFileName (Method)