VisuFctCheckClientSupportsFramePreview (FUN)

FUNCTION VisuFctCheckClientSupportsFramePreview : BOOL

This function checks if client data is not null and the client supports frame swiping with preview. Returns false if clientData is null.

InOut:

Scope

Name

Type

Comment

Return

VisuFctCheckClientSupportsFramePreview

BOOL

Input

pClientData

POINTER TO VisuStructClientData

The client data. Will be checked for null.