TYPE VisuStructInputOnElementEvent : STRUCT
Name
Type
Comment
pClient
POINTER TO VisuStructClientData
A pointer to the client structure were the input occurred.
itfVisualElement
IVisualElement
The visualization element were the input occurred.
eType
VisuEnumInputOnElementType
The type of input that occurred on the element