The EcoStruxure Machine Expert™ – Safety application software is used to develop a functional safety system with a Safety Logic Controller (SLC).
Machine Expert – Safety and therefore also this manual cover different generations of functional safety systems referred to as SLCv1 and SLCv2. The SLCv1 generation includes the TM5CSLC100FS and TM5CSLC200FS, while SLCv2 includes the TM5CSLC300FS and TM5CSLC400FS.
Only the corresponding safety-related modules of the same (firmware) generation can be used with the respective SLC types (since, among other things, the device parameters relevant for the safety response time differ).
This document has been updated with the release of Machine Expert – Safety V2.2.
The technical characteristics of the devices described in this document also appear online. To access this information online, go to the Schneider Electric home page www.se.com.
The characteristics that are described in the present document, as well as those described in the documents included in the Related Documents section below, can be found online. To access the information online, go to the Schneider Electric home page www.se.com/ww/en/download/.
The characteristics that are presented in the present document should be the same as those characteristics that appear online. In line with our policy of constant improvement, we may revise content over time to improve clarity and accuracy. If you see a difference between the document and online information, use the online information as your reference.
Title of Documentation |
Reference Number |
---|---|
Modicon TM5 Safety Logic Controller SLCx00FS Hardware Guide |
EIO0000000889 (Eng) EIO0000000891 (Ger), EIO0000000892 (Ita), |
TM5/TM7 I/O Safety Modules - Hardware Guide |
EIO0000000861 (Eng), EIO0000000862 (Ger), |
Modicon TM7 Digital I/O Modules Hardware Guide |
EIO0000000703 (Eng), EIO0000000704 (Fre), EIO0000000705 (Ger), EIO0000000706 (Spa), EIO0000000707 (Ita), EIO0000000704 (Chs) |
TM5SD••• Instruction Sheet |
S1A85744 |
TM7SDM12DTFS Instruction Sheet |
S1A85745 |
TM5CSLC• /TM5ACSLCM•• Instruction Sheet |
S1A85742 |
TM5CSLC300FS / TM5CSLC400FS / TM5ACSLCM8FS Instruction Sheet |
NNZ96445 |
LMC Pro/Pro2 Hardware Guide |
EIO0000001503 (Eng) EIO0000001504 (Ger) |
TM5 SERCOS III Interface - Hardware Guide |
EIO0000003221 (Eng), EIO0000003222 (Fre), EIO0000003223 (Ger), EIO0000003224 (Spa), EIO0000003225 (Ita), EIO0000003226 (Chs) |
TM5/TM7 Safety Flexible System - System Planning and Installation Guide |
EIO0000001064 (Eng), EIO0000001066 (Ger), |
XY2AU1 / XY2AU1 Instruction Sheet |
163437801A55 (Eng, Ger, Por, Spa, Ita, Fre) |
SlcRemoteController library guide |
EIO0000002149 (Eng), EIO0000002150 (Ger), EIO0000002150 (Ger), EIO0000002150 (Ger), EIO0000002150 (Ger), EIO0000002150 (Ger), EIO0000002150 (Ger), |
M262 Logic/Motion Controller - Programming Guide |
EIO0000003651 (Eng), EIO0000003652 (Fre), EIO0000003653 (Ger), EIO0000003654 (Spa), EIO0000003655 (Ita), EIO0000003656 (Chs) EIO0000003657 (Por) EIO0000003658 (Tur) |
M262 Embedded Safety - Integration Guide |
EIO0000003921 (Eng), EIO0000003923 (Fre), EIO0000003922 (Ger), EIO0000003926 (Spa), EIO0000003924 (Ita), EIO0000003925 (Chs) |
CommonToolbox - Library Guide |
EIO0000004219 (Eng), EIO0000004220 (Fre), EIO0000004221 (Ger), EIO0000004222 (Spa), EIO0000004223 (Ita), EIO0000004224 (Chs) |
Safety Modules - Reference Guide |
EIO0000002265 (Eng), EIO0000002266 (Ger), EIO0000004295 (Ita), |
Safe Logger for Machine Expert Safety - User Guide |
EIO0000002596 (Eng), EIO0000002597 (Ger), EIO0000004361 (Ita), |
Sercos for M262 - User Guide |
EIO0000003883 (Eng), EIO0000003885 (Fre), EIO0000003884 (Ger), EIO0000003888 (Spa), EIO0000003886 (Ita), EIO0000003887 (Chs) |
How to Configure the Firewall for PacDrive LMC Controllers |
EIO0000004198 (Eng) EIO0000004199 (Ger) |
DANGER | |
---|---|
DANGER | |
---|---|
WARNING | |
---|---|
1 |
For additional information, refer to NEMA ICS 1.1 (latest edition), Safety Guidelines for the Application, Installation, and Maintenance of Solid State Control and to NEMA ICS 7.1 (latest edition), Safety Standards for Construction and Guide for Selection, Installation and Operation of Adjustable-Speed Drive Systems or their equivalent governing your particular location. |
WARNING | |
---|---|
Pay particular attention in conforming to any safety information, different electrical requirements, and normative standards that would apply to your adaptation.
WARNING | |
---|---|
For reasons of Internet security, for those devices that have a native Ethernet connection, TCP/IP forwarding is disabled by default. Therefore, you must manually enable TCP/IP forwarding. However, doing so may expose your network to possible cyberattacks if you do not take additional measures to protect your enterprise. In addition, you may be subject to laws and regulations concerning cybersecurity.
WARNING | |
---|---|
Consult the Schneider Electric Cybersecurity Best Practices for additional information.
The technical terms, terminology, symbols and the corresponding descriptions in this manual, or that appear in or on the products themselves, are generally derived from the terms or definitions of international standards.
In the area of functional safety systems, drives and general automation, this may include, but is not limited to, terms such as safety, safety-related function, safe-state, fault, fault reset, malfunction, failure, error, error message, dangerous, etc.
Among others, these standards include:
Standard |
Description |
---|---|
IEC 61131-2:2008 |
Programmable controllers, part 2: Equipment requirements and tests. |
ISO 13849-1:2015 |
Safety of machinery: Safety related parts of control systems. General principles for design. |
EN 61496-1:2021 |
Safety of machinery: Electro-sensitive protective equipment. Part 1: General requirements and tests. |
ISO 12100:2010 |
Safety of machinery - General principles for design - Risk assessment and risk reduction |
EN 60204-1:2019 |
Safety of machinery - Electrical equipment of machines - Part 1: General requirements |
ISO 14119:2013 |
Safety of machinery - Interlocking devices associated with guards - Principles for design and selection |
ISO 13850:2015 |
Safety of machinery - Emergency stop - Principles for design |
IEC 62061:2019 |
Safety of machinery - Functional safety of safety-related electrical, electronic, and electronic programmable control systems |
IEC 61508-1:2011 |
Functional safety of electrical/electronic/programmable electronic safety-related systems: General requirements. |
IEC 61508-2:2010 |
Functional safety of electrical/electronic/programmable electronic safety-related systems: Requirements for electrical/electronic/programmable electronic safety-related systems. |
IEC 61508-3:2011 |
Functional safety of electrical/electronic/programmable electronic safety-related systems: Software requirements. |
IEC 61784-3:2022 |
Industrial communication networks - Profiles - Part 3: Functional safety fieldbuses - General rules and profile definitions. |
2006/42/EC |
Machinery Directive |
2014/30/EU |
Electromagnetic Compatibility Directive |
2014/35/EU |
Low Voltage Directive |
In addition, terms used in the present document may tangentially be used as they are derived from other standards such as:
Standard |
Description |
---|---|
IEC 60034 series |
Rotating electrical machines |
IEC 61800 series |
Adjustable speed electrical power drive systems |
IEC 61158 series |
Digital data communications for measurement and control – Fieldbus for use in industrial control systems |
Finally, the term zone of operation may be used in conjunction with the description of specific hazards, and is defined as it is for a hazard zone or danger zone in the EC Machinery Directive (2006/42/EC) and ISO 12100:2010.
The aforementioned standards may or may not apply to the specific products cited in the present documentation. For more information concerning the individual standards applicable to the products described herein, see the characteristics tables for those product references.
If not otherwise stated, the respective terms are used in keeping with the IEC 61508 standard.
"Error" in keeping with the common use in the context of programming systems. Machine Expert – Safety helps to detect invalid code syntax, programmed by the user, qualifies them as errors and outputs accordingly an error message in the Machine Expert – Safety message window.
"Standard" = non-safety-related (according to IEC 61508 and PLCopen TC5 Safety Specification V1.0). The term "standard" always refers to non-safety-related items. Examples: a standard process data item is only read/written by a non-safety-related I/O device (that is to say, a standard device). Standard variables/functions/function blocks are non-safety-related data. The term "standard PLC" designates the non-safety-related controller.
"Non-safe" as synonym for "standard" (only in the Machine Expert – Safety Error Catalog, message text as displayed in Machine Expert – Safety), taking the PLCopen TC5 Safety Specification V1.0 into account.