XOR / XOR_S - XOR connection

This bitwise Boolean function realizes a logical exclusive-OR-integration of the operands connected to the input parameters. The function is available as standard function XOR and safety-related function XOR_S.

XOR

Parameter

Data types

Description

IN1

ANY_BIT

First input value

IN2

ANY_BIT

Second input value

OUT

ANY_BIT

Output value

XOR_S

Parameter

Data types

Description

IN1

ANY_SAFEBIT

First input value

IN2

ANY_SAFEBIT

Second input value

OUT

ANY_SAFEBIT

Output value

NOTE:

All parameters must have the same data type.