ET_Transformation

 

ET_Transformation - General Information

Overview

Type:

Enumeration type

Available as of:

V1.0.0.0

Description

Type of the kinematics/transformation of the robot.

Enumeration Elements

Name

Value

Description

None

0

The kinematics/transformation of the robot is not defined yet.

Cartesian2AxXY

10

Biaxial Cartesian robot that works in the Cartesian XY plane.

Cartesian2AxXZ

11

Biaxial Cartesian robot that works in the Cartesian XZ plane.

Cartesian2AxYZ

12

Biaxial Cartesian robot that works in the Cartesian YZ plane.

Cartesian3Ax

20

Triaxial Cartesian robot.

Delta3Ax

30

Triaxial Delta robot.

User3Ax

40

An up to three axial user-configured transformation.

Delta2AxXY

50

Biaxial Delta robot that works in the Cartesian XY plane.

Delta2AxXZ

51

Biaxial Delta robot that works in the Cartesian XZ plane.

Delta2AxYZ

52

Biaxial Delta robot that works in the Cartesian YZ plane.

Articulated2AxXY

60

Biaxial Articulated robot that works in the Cartesian XY plane.

Articulated2AxXZ

61

Biaxial Articulated robot that works in the Cartesian XZ plane.

Articulated2AxYZ

62

Biaxial Articulated robot that works in the Cartesian YZ plane.

Scara4Ax

70

SCARA with four axes.

Gantry2AxXY

80

Gantry transformation for two axes (working plane XY).

Gantry2AxXZ

81

Gantry transformation for two axes (working plane XZ).

Gantry2AxYZ

82

Gantry transformation for two axes (working plane YZ).

User6Ax

90

An up to six axial user-configured transformation.