IF_RobotFeedbackMotionOrientation

 

IF_RobotFeedbackMotionOrientation - General Information

Overview

Type:

Interface

Available as of:

V2.8.2.0

Inherits from:

IF_RobotFeedbackMotionRefActualValues

This chapter provides information on:

oTask

oDescription

oProperties

Task

Interface with return values of an orientation.

Description

This interface is part of IF_RobotFeedback and contains data on an active orientation motion.

Properties

Name

Data type

Accessing

Description

etMovementMode

ET_MovementMode

Read

Movement mode of the orientation of the active motion job.

lrEstimatedStopPosition

LREAL

Read

Estimated stop position of the orientation movement.

udiCurrentMovementId

UDINT

Read

Movement Id of the active motion job of the orientation.

udiNextMovementId

UDINT

Read

Movement Id of the motion job of the orientation that is executed after the active motion job.

udiPreviousMovementId

UDINT

Read

Movement Id of the motion job of the orientation that was executed before the active motion job.

xInMotion

BOOL

Read

TRUE = The orientation is in motion.

FALSE = The orientation is at standstill.

xInTarget

BOOL

Read

TRUE = The orientation is in the target position of the last motion job.

FALSE = The orientation is not in the target position of the last motion job.

For further information on properties, refer to IF_RobotFeedbackMotionRefActualValues.