ST_TrackingParameters

 

ST_TrackingParameters - General Information

Overview

Type:

Data structure

Available as of:

V2.14.0.0

Inherits from:

-

Description

Structure to describe additional parameters for a tracking system.

Also refer to Minimizing the Influence of a Tracking System on the Trajectory of a Robot.

Structure Elements

Variable

Data type

Description

lrAccelerationZeroThreshold

LREAL

This value defines an acceleration limit for a tracking system. For accelerations below this limit, the state of the tracking system is treated as constant velocity or standstill during desynchronization phase.

Valid values are:

olrAccelerationZeroThreshold ≥ 0.0

olrAccelerationZeroThreshold = -1.0

To disable the detection of standstill or constant velocity set the value to -1.0.

NOTE: Modifying the value for a tracking system via the method SetTrackingParameters() while the tracking system is active during the call of the method, is only taken into account after leaving and reentering the tracking system.