IF_Robot

 

IF_Robot - General Information

Overview

Type:

Interface

Available as of:

V1.0.0.0

Inherits from:

-

This chapter provides information on:

oTask

oDescription

oProperties

Task

Interface for controlling the FB_Robot.

Description

This interface is implemented by the function block FB_Robot.

NOTE: For Modicon M262 Motion Controllers: If FB_Robot and/or IF_Robot report a diagnostic message and the axis is in MOIN.ET_AxisState.ErrorStop state, FB_Robot and/or IF_Robot must be disabled and MC_Reset must be executed to reset the axis.

Properties

Name

Data type

Accessing

Description

etDiag

GD.ET_Diag

Read

General library-independent statement on the diagnostic.

A value unequal to GD.ET_Diag.Ok corresponds to a diagnostic message.

etDiagExt

ET_DiagExt

Read

POU-specific output on the diagnostic.

q_etDiag = GD.ET_Diag.Ok -> Status message

q_etDiag <> GD.ET_Diag.Ok -> Diagnostic message

ifConfiguration

IF_RobotConfiguration

Read

Interface for the robot configuration.

ifFeedback

IF_RobotFeedback

Read

Interface with return values.

ifJogging

IF_RobotJogging

Read

Interface for manual motion of the robot.

ifMotion

IF_RobotMotion

Read

Interface for motion programming.

sMsg

STRING[80]

Read

Event-triggered message that gives more detailed information on the diagnostic state.

xActive

BOOL

Read

TRUE: The POU is active and has to be executed further.

FALSE: The POU is inactive.

xDiagQuit

BOOL

Read/Write

A rising edge FALSE -> TRUE acknowledges the following diagnostic messages:

oetDiag = GD.ET_Diag.ConfigurationFailed

oetDiagExt = ET_DiagExt.ConfigInvalid

xEnable

BOOL

Read/Write

A rising edge FALSE -> TRUE activates the POU, a falling edge TRUE -> FALSE deactivates the POU.

A deactivated POU does not execute any actions.

xReady

BOOL

Read

TRUE: The POU is ready to operate and can accept user commands.

FALSE: The function block is not ready to accept user commands.

xStart

BOOL

Read/Write

TRUE: Motion commands issued via the IF_RobotMotion interface are started.

FALSE: Active motions are stopped and can be continued by setting xStart: = TRUE again. The robot can be positioned via the IF_RobotJogging interface.

xWsSelect

BOOL

Read/Write

TRUE: A warm start motion is pre-selected.

xWsStart

BOOL

Read/Write

TRUE: If xWsSelect = TRUE, the robot moves to the last detected path position.

To perform a warm start, it is necessary to re-enable the FB_Robot by setting xEnable to FALSE and TRUE again.