(American wire gauge) The standard that specifies wire section sizes in North America.
A mounting device that is designed to seat an electronic module on a DIN rail and connect it to the TM5 bus for M258 and LMC058 logic controllers. Each base bus extends the integrated TM5 data and electronic power buses as well as the 24 Vdc I/O power segment. The electronic modules are added to the TM5 system through their insertion on the base bus.
Connectors that have 1 raised key on the female connector and 1 mating slot on the male connector. These connectors (also called reverse keyed) are used for Sercos bus applications.
The arrangement and interconnection of hardware components within a system and the hardware and software parameters that determine the operating characteristics of the system.
(Canadian standards association) The Canadian standard for industrial electronic equipment in hazardous environments.
(Deutsches Institut für Normung) A German institution that sets engineering and dimensional standards.
(electronic industries alliance) The trade organization for establishing electrical/electronic and data communication standards (including RS-232 and RS-485) in the United States.
In a programmable controller system, most electronic modules directly interface to the sensors, actuators, and external devices of the machine/process. This electronic module is the component that mounts in a bus base and provides electrical connections between the controller and the field devices. Electronic modules are offered in a variety of signal levels and capacities. (Some electronic modules are not I/O interfaces, including power distribution modules and transmitter/receiver modules.)
EN identifies one of many European standards maintained by CEN (European Committee for Standardization), CENELEC (European Committee for Electrotechnical Standardization), or ETSI (European Telecommunications Standards Institute).
A device for length or angular measurement (linear or rotary encoders).
A part of a machine including sub-assemblies such as conveyors, turntables, and so on.
An electronic communication bus between expansion I/O modules and a controller or bus coupler.
FAST input/output Specific I/O modules with some electrical features (for example, response time) while the treatment of these channels are done directly by the controller
(functional Earth) A common grounding connection to enhance or otherwise allow normal operation of electrically sensitive equipment (also referred to as functional ground in North America).
In contrast to a protective Earth (protective ground), a functional earth connection serves a purpose other than shock protection, and may normally carry current. Examples of devices that use functional earth connections include surge suppressors and electromagnetic interference filters, certain antennas, and measurement instruments.
Represents the BIOS, data parameters, and programming instructions that constitute the operating system on a controller. The firmware is stored in non-volatile memory within the controller.
A programming unit that has 1 input and returns 1 immediate result. However, unlike FBs, it is directly called with its name (as opposed to through an instance), has no persistent state from one call to the next and can be used as an operand in other programming expressions.
Examples: boolean (AND) operators, calculations, conversions (BYTE_TO_INT)
(identifier/identification)
(international electrotechnical commission) A non-profit and non-governmental international standards organization that prepares and publishes international standards for electrical, electronic, and related technologies.
(Internet protocol Part of the TCP/IP protocol family that tracks the Internet addresses of devices, routes outgoing messages, and recognizes incoming messages.
(ingress protection) The protection classification according to IEC 60529 offered by an enclosure, shown by the letter IP and 2 digits. The first digit indicates 2 factors: helping protect persons and for equipment. The second digit indicates helping protect against water. IP 20 devices help protect against electric contact of objects larger than 12.5 mm, but not against water.
(ingress protection) The protection classification according to IEC 60529. IP 67 modules are protected against ingress of dust, contact, and water up to an immersion depth of 1 m.
(light emitting diode) An indicator that illuminates under a low-level electrical charge.
(millisecond)
(national electrical manufacturers association) The standard for the performance of various classes of electrical enclosures. The NEMA standards cover corrosion resistance, ability to help protect from rain, submersion, and so on. For IEC member countries, the IEC 60529 standard classifies the ingress protection rating for enclosures.
A system of interconnected devices that share a common data path and protocol for communications.
(power distribution module) A module that distributes either AC or DC field power to a cluster of I/O modules.
(Protective Earth) A common grounding connection to help avoid the hazard of electric shock by keeping any exposed conductive surface of a device at earth potential. To avoid possible voltage drop, no current is allowed to flow in this conductor (also referred to as protective ground in North America or as an equipment grounding conductor in the US national electrical code).
A command that causes the controller to scan the application program, read the physical inputs, and write to the physical outputs according to solution of the logic of the program.
(serial real-time communications system) A digital control bus that interconnects, motion controls, drives, I/Os, sensors, and actuators for numerically controlled machines and systems. It is a standardized and open controller-to-intelligent digital device interface, designed for high-speed serial communication of standardized closed-loop real-time data.
A command that causes the controller to stop running an application program.
(terminal block) The component that mounts in an electronic module and provides electrical connections between the controller and the field devices.
(underwriters laboratories) A US organization for product testing and safety certification.