The Multicarrier library provides functions for controlling the multi carrier transport system.
The library covers the following tasks:
Moving individual carriers
Synchronizing the movements of carriers
Superimposing motions on running carrier movements
Synchronizing carrier motion with external movements
Avoiding collisions
The table indicates the characteristics of the library:
Characteristic |
Value |
---|---|
Library name |
Multicarrier |
Company |
Schneider Electric |
Category |
|
Component |
multi carrier |
Default namespace |
|
Language model attribute |
|
Forward compatible library (FCL) |
Yes (FCL) |
In conjunction with the library, the example project Multicarrier Example is provided. The example project demonstrates how to implement the components from the Multicarrier library.
The example project is installed on your PC along with the programming software. To open the project example, proceed as follows:
Step |
Action |
Comment |
---|---|---|
1 |
In the EcoStruxure Machine Expert Logic Builder, execute the command . |
– |
2 |
In the dialog box, select from the list. |
– |
3 |
On the right-hand side of the dialog box, click the button . |
Result: Available examples are listed in the drop down menu. |
4 |
Select your example from the drop down menu. |
– |
5 |
Select your controller from the list. |
– |
6 |
Enter a name for the new project, and select the file location. |
– |
7 |
Click the button. |
Result: A new project is created based on the selected example. |