SMC_AdaptHelpMarks (FUN)

FUNCTION SMC_AdaptHelpMarks : SMC_ERROR

Adapts the help marks if a new element has been inserted between two existing elements. The help marks are moved to the new element if they no longer fit on the cut first and second object. This is done so that the following constraints are met, where the second constraint beats the first one if both cannot be met:

  1. The distance of the h-function stays the same as for the original (uncut) elements. For the first element, the distance is measured from the start point. For the second element, the distance is measured from the end point.

  2. The h-function is moved no further than to the middle of the new element.

Note

Note that constraint 2 makes sure that the order of h-functions does not change compared to the original elements.

Note

When a mark is to be adapted to a new path element whose iHelpID array is already full (MAX_IPOSWITCHES) then an error SMC_PATH_MAX_HPOINTS_EXCEEDED is produced

InOut:

Scope

Name

Type

Comment

Return

SMC_AdaptHelpMarks

SMC_ERROR

Inout

gi1

SMC_GeoInfo

The first element

giN

SMC_GeoInfo

The new element

gi2

SMC_GeoInfo

The second element

Input

l1Orig

LREAL

The original length of the first element

l2Orig

LREAL

The original length of the second element