|
Input
|
wOUTQUEUEStructID
|
WORD
|
16#9878
|
The fix value of this variable allows to check if the provided structure variable is of type SMC_OUTQUEUE.
|
|
pbyBuffer
|
POINTER TO ARRAY [0..0] OF SMC_GeoInfo
|
|
Address of coherent memory buffer allocated for SMC_GEOINFO objects. The variable pbyBuffer has to be assigned in every cycle within the IEC program allocating the buffer. The allocation is done within the declaration part, e.g. by using an array (BUFFER: ARRAY [0..99] OF SMC_GEOINFO for a memory area large enough to hold 100 SMC_GEOINFO objects).
|
|
nCapacity
|
UDINT
|
|
Contains the capacity in multiples of SMC_GEOINFO objects (The number OF SMC_GEOINFO objects that fit into pbyBuffer). The function SMC_SetQueueCapacity initializes this field.
|
|
nReadPos
|
UDINT
|
|
Contains the position in multiples of SMC_GEOINFO objects of the first object in the list.
|
|
bEndOfList
|
BOOL
|
|
In order to avoid a buffer underrun ( SMC_Interpolator), the SoftMotion function block being passed an SMC_OUTQUEUE structure will not start with the processing of this queue, until it has been filled up completely. However, when working on the last SMC_GEOINFO objects of a path, SMC_OUTQUEUE is no longer complete. Hence, in order to keep the processing going on, bEndOfList has to be set to TRUE as soon as the last SMC_GEOINFO object has been stored. In case that the list will be empty hereafter, but should be filled up again, bEndOfList has to be reset to FALSE.
|
|
byGenerator
|
BYTE
|
250
|
Originator of the queue. The interpolator will use this information for verifying that SMC_CheckVelocities has been processed as prescribed.
Valid values are:
|
|
bReCheckVelocities
|
BOOL
|
|
Internal variable
|
|
strProgramName
|
STRING
|
|
Name of the CNC program
|
|
nWritePos
|
UDINT
|
|
Contains the next free position in multiples of SMC_GEOINFO objects. (Declared after strProgramName in order to avoid cache thrashing: make sure, nReadPos and nWritePos aren't part of the same cache line.))
|
|
xPartofLM
|
BOOL
|
|
If the input, generated by programming system, is TRUE, the function block is maintained by managers.
|
|
nNumReservedEntries
|
UDINT
|
|
The number of reserved entries: if this number of free entries is reached, SMC_OutQueue.bFull will return TRUE. Must be at least 3 and at most nCapacity-1.
|
|
nPastMarker
|
DINT
|
|
Points to the first element that has been stored in the queue (if any) and has not yet been overwritten. So the elements from nPastMarker to nReadPos-1 are the "past" of the current queue. nPastMarker equals -1 if (and only if) no element has been appended to the queue yet.
|