Type |
AK |
Devices supporting the parameter |
Bus terminals BT-4/DIO1 and BT-4/DIO1 TP, Bus terminal BT-4/ENC1 |
Traceable |
No |
Reads out the version number of the bus terminal.
NOTE: The value is read out once when the system starts and is not updated afterward.
Value |
Data type |
Meaning |
---|---|---|
xxxxx |
STRING (20) |
The firmware version was determined and is displayed in the parameter. |
Virtual |
STRING (20) |
The bus address of the bus terminal is in the PLC configuration >= 100. |
unavailable |
STRING (20) |
The firmware version could not be determined. Causes: oBus error detected oHardware does not support reading the version |