METHOD UpdateConfiguredIPSettings : ErrorCode
This method updates the configured ip address, subnet mask and standard gateway of the ethernet node. The device has to be in disabled state (via Enable, see also DED.Reconfigure), else the update is rejected.
InOut: |
|