SMC_POSINFO (STRUCT)

TYPE SMC_POSINFO : STRUCT

This data type describes its coordinates and the positions of the additional axes for a particular position point.

InOut:

Name

Type

Initial

Comment

iFrameNo

INT

0

In this variable additional information not relevant for the SoftMotion modules may be stored by the user.

wAuxData

WORD

7

Bit by bit description of position axis to be calculated by the SMC_Interpolator. Its initialization with 2#111 causes the X, Y and Z axes to be interpolated. The first bit set will effect the calculation of the dX position, whereas the seventh bit for example will effect a processing of dA2.

wSProfile

WORD

0

Analogously to wAuxData, the value of wSProfile prescribes whether the additional axes, i.e. other than the X or Y axis, shall be interpolated in linear (FALSE) or sigmoid (S-) shape (TRUE) with constant jerk. Bit2 refers to the Z axis, Bit6 to P, Bit7 to Q, Bit8 to U, Bit9 to V and Bit10 to W.

dX

LREAL

0

X-position in coordinate system

dY

LREAL

0

Y-position in coordinate system

dZ

LREAL

0

Z-position in coordinate system

dA

LREAL

0

Currently not used

dB

LREAL

0

Currently not used

dC

LREAL

0

Currently not used

dA1

LREAL

0

Position of additional axis P

dA2

LREAL

0

Position of additional axis Q

dA3

LREAL

0

Position of additional axis U

dA4

LREAL

0

Position of additional axis V

dA5

LREAL

0

Position of additional axis W

dA6

LREAL

0

Position of additional axis A6 (Cannot be programmed with G-code!)