This help chapter contains topics that describe all necessary steps and procedures for programming a project.
You will learn how to:
Open and import/export safety-related projects.
Parameterize used devices using the Device Parameterization Editor and what are Advanced and Commissioning Parameters.
Define the project structure in the project tree by managing logical POUs and libraries.
Program the Enable Principle.
Edit code in the graphical IEC 61131 programming languages FBD and LD.
Descriptions of the available code objects and the dialogs used to edit these objects can be found in the related topics provided in the "User Interface" help chapter.
Edit code in the textual IEC 61131 programming language ST.
Set the POU verification flag after having completed and verified a user POU in order to protect it against unintended modifications and to indicate its state in the project tree.
After having edited the project, continue with
Term definition: Standard = non-safety-related.
The term "standard" always refers to non-safety-related items/objects. Examples: a standard process data item is only read/written by a non-safety-related I/O device, i.e., a standard device. Standard variables/functions/FBs are non-safety-related data. The term "standard controller" designates the non-safety-related controller.
Machine Expert - Safety provides a certification manager for certifying the completed project after successful commissioning. A certified project is protected by password against modifications. (Such modifications would result in a new project acceptance procedure and certification.)
If you can't edit the project although you are logged-on correctly, verify whether the project is already certified. This is indicated in the status bar (rightmost):
Refer to the topic "Project certification" for detailed information.