|
Inout
|
sentences
|
SMC_GSentenceQueue
|
|
The input queue of g-code sentences
|
|
Input
|
bExecute
|
BOOL
|
|
Execution starts on the rising edge.
|
|
bAbort
|
BOOL
|
|
If TRUE, the current processing of this function block is aborted
|
|
bAppend
|
BOOL
|
|
If TRUE, a rising edge of bExecute won't lead to a reset of the out-queue. Instead, newly incoming data will be written to the end of the out-queue.
|
|
piStartPosition
|
SMC_POSINFO
|
|
Start position of the path.
|
|
vStartToolLength
|
SMC_Vector3d
|
|
Start tool length.
|
|
nSizeOutQueue
|
UDINT
|
|
This variable contains the size of the data buffer, the list of SMC_GEOINFO structure objects will be written to. This buffer must be able to hold at least five SMC_GEOINFO objects. Otherwise, the function block will not execute any actions at all. Its size may be predefined, but may be modified later only during a reset. It is recommended to create the buffer as described by the example below:
ExampleBuf: Array[1..50] of SMC_GeoInfo;
The appropriate buffer size will then be retrieved by use of the operator sizeof(ExampleBuf).
|
|
pbyBufferOutQueue
|
POINTER TO ARRAY [0..0] OF SMC_GEOINFO
|
|
This input must point to the first byte of the memory area that is allocated for the SMC_OUTQUEUE structure. This area must be at least as big as defined in nSizeOutQueue. Typically the allocation of the memory buffer is done in the declaration part of the IEC-program by defining an array of SMC_GEOINFO (e.g. BUF: ARRAY[1..50] OF SMC_GEOINFO; for a buffer that can store 50 path elements). The value may be predefined, but may be modified later on only during a reset.
|
|
bEnableSyntaxChecks
|
BOOL
|
TRUE
|
Turns on syntax checks that will detect invalid G-code and stop with an error in this case. It is recommended to use the syntax checks.
|
|
eOriConv
|
SMC_ORI_CONVENTION
|
SMC_ORI_CONVENTION.ADDAXES
|
Defines the way the orientation in the A/B/C words is interpreted.
For movement commands (such as G01, G02, ...), the value determines how A/B/C are treated. For values other than SMC_ORI_CONVENTION.``ADDAXES``, the angles A/B/C may be normalized, even if no coordinate rotation has been programmed. For example with orientation convention ZYZ, a programmed orientation of A=90° B=0° C=0° may result in the (equivalent) rotation A=0° B=0° C=90° in the path element.
For commands that set the decoder coordinate system (G54/G55/G56), the value determines how the coordinates A/B/C are treated. If the value is SMC_ORI_CONVENTION.``ADDAXES``, then A/B/C are treated as independent additional axes, for which offsets are set. For all other values, A/B/C are treated as an orientation, and the decoder coordinate system is rotated accordingly.
Note
If used with tool correction functions such as SMC_ToolLengthCorr, the same orientation convention has to be used there.
|
|
dCircleTolerance
|
LREAL
|
|
|
Tolerance to decide whether the definition of a circle makes sense.
|
-
case definition via target-position and radius: If the distance between start- and end-position (both projected onto the circle plane) is greater than 2 * the radius + MAX(fCircleTolerance, 1e-06), the circle will be converted into a line.
-
case definition via target- and center-position: Let x be the maximum of the distance between start- and center-position and the distance between target- and center-position (projecting everything onto the circle plane). If those distances differ by more than MAX(fCircleTolerance, 0.1 * x), the circle will be converted into a line.
|
|
|
pInterpreterStack
|
POINTER TO BYTE
|
|
Allows to supply a buffer for the interpreter stack. If 0, a default buffer of size 10240 Bytes is used. If <> 0, the given buffer will be used. This input is read each cycle.
|
|
nInterpreterStackSizeBytes
|
UDINT
|
|
The size of the buffer pointed to by pInterpreterStack. Note that the size needs to be at least 1024 Bytes.
|
|
Output
|
bDone
|
BOOL
|
|
This variable will be set to TRUE as soon as the input data has been processed completely. The function block will not perform any further actions until it gets reset.
|
|
bBusy
|
BOOL
|
|
TRUE, while execution of function block is not finished.
|
|
bError
|
BOOL
|
|
Signals that an error has occurred within the function block.
|
|
wErrorID
|
SMC_ERROR
|
|
Error identification
|
|
errorPos
|
SMC_NC_SourcePosition
|
|
The source-position where an error has been detected.
|
|
poqDataOut
|
POINTER TO SMC_OUTQUEUE
|
|
Pointer to the SMC_OUTQUEUE structure that manages the decoded SMC_GEOINFO objects.
|
|
iStatus
|
SMC_DEC_STATUS
|
|
The current status.
|
|
iLineNumberDecoded
|
DINT
|
|
The variable contains the 0-based line number of the CNC file.
|
|
GCodeText
|
SMC_GCODE_TEXT
|
|
The G-Code text.
|
|
CallstackInfo
|
SMC_NCCallstackInfo
|
|
|
|
aActivePrograms
|
ARRAY [0..(SoftMotion_NC2_Constants.IPR_CALLSTACK_SIZE - 1)] OF STRING
|
|
The currently active programs and subprograms. aActivePrograms[0] holds the name of the (sub)program that is currently interpreted. If it is a sub-program, then aActivePrograms[1] holds the name of the calling (sub)program and so on. The list of active programs is terminated by an empty string.
|