METHOD GetSlaveActivation : UDINT
Method GetSlaveActivation is part of the interface ICmpIoDrvPbSlaveActivation. It is can be used in the application to get information on the current state of slave activation. See documentation of PB_SlaveActivation in IoDriver Profibus2 Interface Library for further information.
InOut: |
|