Module_Diag.SetCommunicationState (METH)

METHOD SetCommunicationState : DED.ERROR

Starts, stops or resets a device

Note

Use |IDevice2.CheckSupportedCommunicationState| and |IDevice2.CheckCurrentSupportedCommunicationState| to check which transitions are possible!

InOut:

Scope

Name

Type

Comment

Return

SetCommunicationState

DED.ERROR

Input

eRequestedState

DED.DEVICE_TRANSITION_STATE

desired transition