METHOD GetProgramName : STRING(255)
The name of the program or subprogram. This is usually the full path of the CNC file. E.g. for the file with full path '/some/dir/name.cnc'.
Scope
Name
Type
Return
GetProgramName
STRING(255)