Constant
|
TABLE_UPPER_BOUND
|
INT
|
15
|
size of table for AnalyzeExpressionTable and AnalyzeExpressionTableEx
|
STRING_LENGTH_EXP
|
INT
|
255
|
string length of one entry in table (variable or complex expression)
|
STRING_LENGTH_ADDRESS
|
INT
|
20
|
string length for address in table
|
|
INT
|
255
|
string length of comment in table
|
STRING_LENGTH_OUTSTRING
|
INT
|
255
|
string length of string output for AnalyzeExpression and AnalyzeExpressionCombined and AnalyzeExpressionCombinedEx
|
TABLE_SHOW_VALID_ITEMS
|
BOOL
|
FALSE
|
if TRUE, also valid items are added to the table, and the failed-entry of the table is filled correspondingly if FALSE, only failed items are added to the table and the failed-entry of the table is always true
|