FUNCTION_BLOCK FINAL BackgroundTask EXTENDS FBF.InstanceBase IMPLEMENTS IBackgroundTask, ICmpEventCallback
Encapsulates all the details of managing a iec task in the context of the runtime system.
A running background task can be controlled via the methods of IBackgroundTask.
| Watchdog Sensitivity: |
If the actual cycle time of a task exceeds the currently udiWatchdogTime, the currently defined usiWatchdogSensitivity value is taken into account:
|
| InOut: |
|
Properties:
Methods:
Structure: