Hysteresis_DINT (FB)

FUNCTION_BLOCK Hysteresis_DINT

This function block will set the output variable to TRUE, if the integral value is smaller than an integral lower bound

It will set the Boolean output variable to FALSE, if the input value exceeds the integral upper bound .

If lies between the lower and upper bound, the value of the output will rest unchanged by the module.

InOut:

Scope

Name

Type

Comment

Input

diValue

DINT

input value

diLimitPos

DINT

upper bound

diLimitNeg

DINT

lower bound

Output

xOut

BOOL

FALSE: If

TRUE: If

xOut” else