CHECK
|
0
|
If the Field Device interface has received a request to provide a process data record, only the outputs NEW, SLOT, INDEX and RLEN are set. Multiple calls of this function block with MODE=0 returns the outputs for the same request.
|
RECEIVE
|
1
|
If the Field Device interface has received a request, the function block outputs are updated.
|
RECEIVE_BY_SLOT
|
2
|
If the Field Device interface has received a request for the slot and subslot the numbers of which are given in F_ID input, the function block outputs are updated.
|
POS_RESPONSE
|
3
|
After checking or receiving the request to provide a process data record, this function block provides the requested process data record with its RECORD parameter and sends a positive response to the Host Controller.
|
NEG_RESPONSE
|
4
|
After checking or receiving the request to provide a process data record, this function block refuses to provide this record and sends a negative response to the Host Controller. The error reason is given with the inputs CODE1 and CODE2.
|