FUNCTION WREPLACE : WSTRING(255)
Replaces L wcharacters of STR1 by STR2, starting at the POS-th wcharacter position and returns the new string. POS = 1 is the first character.
The current implementation is unfortunately not correct for the case P=0. The implementation cannot be changed for compatibility reasons.
If P=0 is used, the parameter L is internally reduced by one!
It is generally recommended to use values in the range specified by IEC 61131-3. The smallest value for P is specified there as 1.
InOut: |
|