|
g_pVisuTextBuffer
|
POINTER TO ARRAY [0..Visu_Constants.VISU_TEXTBUFFER_SIZE] OF WORD
|
|
Is used when size is configured
|
|
g_iConfiguredTextBufferSize
|
INT
|
-1
|
|
|
g_VisuManager
|
IVisuManager2
|
g_VisuManager_Inst
|
could be used by endusers too -> visible
|
|
g_SelectionManager
|
ISelectionManager
|
g_SelectionManager_Inst
|
could be used by endusers too -> visible
|
|
g_VisualizationStyle
|
IVisualizationStyle
|
Private_Visu_Globals.g_VisualizationStyle_Dummy_Inst
|
initialized with a private dummy instance to prevent having NULL values; qualified due to a current limitaion of the ieccodeconverter
|
|
g_VisuRectangleProvider
|
IApplicationRectangleProvider
|
0
|
If an instance is assigned to this variable, then this instance will be called whenever a new list of touch rectangles is built.
|
|
CURRENTVISU
|
STRING
|
‘’
|
will be used only if the settings activate them
@IECCodeConverter_Type: String
|
|
CURRENTLANGUAGE
|
STRING
|
‘’
|
is always active
|
|
CurrentUserGroupId
|
DWORD
|
|
Visu user mgmt variables - only necessary for target clients
CHECKED_OMIT
|
|
CurrentUserGroupName
|
WSTRING(511)
|
|
CHECKED_OMIT
|
|
CurrentUserName
|
WSTRING
|
“None”
|
CHECKED_OMIT
|
|
CurrentFullUserName
|
WSTRING
|
“None”
|
CHECKED_OMIT
|
|
CurrentUseAutoLogoutTime
|
BOOL
|
|
CHECKED_OMIT
|
|
CurrentRemainingAutoLogoutTime
|
TIME
|
|
Only valid if CurrentUseAutoLogoutTime is TRUE.
|
|
CurrentClientType
|
Visu_ClientType
|
|
CHECKED_OMIT
|
|
VISU_CYCLE_TIME_ON_OPEN_DIALOGS
|
UDINT
|
1000
|
Settings for performance optimizatin on open dialogs
|
|
OPEN_DIALOGS_DISABLE_CHANGING_INVALIDATION_RECT
|
BOOL
|
FALSE
|
|
|
g_VisuKineticScrollingSizeFactor
|
REAL
|
1.0
|
|
|
g_VisuKineticScrollingDamping
|
REAL
|
0.1
|
|
|
g_VisuTouchScrollingOutsideElem
|
BOOL
|
FALSE
|
|
|
g_VisuLineJoinMiterLimit
|
REAL
|
1.5
|
|
|
g_MaxTwoDigitYear
|
UINT
|
2099
|
|
|
g_DateTimeValuesInIECSyntax
|
BOOL
|
FALSE
|
|
|
g_VisuRedundSyncFrameIndex
|
BOOL
|
FALSE
|
Set the behavior of how to syncronize the frames indexes in during visu redundancy
|
|
g_VisuRedundValueChanged
|
VisuEnumRedundancyValueChanged
|
VisuEnumRedundancyValueChanged.OnlySyncArea
|
Set the action to do when in visu redundancy we change a visu variable on the active device.
|
|
SECURE_TAPPING_TIMEOUT
|
DWORD
|
2000
|
Timeout in ms for secure tapping. If there is no connection for this period of time, all current Tap actions are automatically terminated.
|
|
g_xForceDlgPosAsDesigned
|
BOOL
|
|
How to handle the position of dialog box when no valid previous position has been found
|
|
g_xUseGlobalDlgPos
|
BOOL
|
TRUE
|
Allow to use the global dialog position when a new client is opened
|
|
g_VisuTrendWithTimeSelectorUpdateBehaviour
|
UINT
|
100
|
For a trend with time selector: The update rate can be dependent on the value of the time selector Value 0: Update rate not dependent on time selector value. Feature is not used. Values > 0: Update rate dependent on time selector value. Update rate of trend will be: time selector value / g_VisuTrendWithTimeSelectorUpdateBehaviour (Hint: A update, faster than the visu task is not possible. Also a update rate less than ms is not possible)
|