FUNCTION VisuFctIsRectRotatedBy0To90Degree : BOOL
Checks if a rectangle is rotated by a degree in the range of 0 - 90
Scope
Name
Type
Return
VisuFctIsRectRotatedBy0To90Degree
BOOL
Input
rect
VisuStructPaintRectangle