About this help

This help discusses features of the PowerLogic™ ION7400 series power meter and provides configuration instructions.

Throughout the help, the term “meter” refers to all models of the PowerLogic™ ION7400 series meter. All differences between the models, such as a feature specific to one model, are indicated with the appropriate model number or description.

Assumptions

This help assumes you have an understanding of power metering and are familiar with the equipment and power system in which your meter is installed.

This help does not provide configuration information for advanced features where an expert user would perform advanced configuration. It also does not include instructions on how to incorporate meter data or perform meter configuration using energy management systems or software, other than ION Setup. ION Setup is a free configuration tool available for download from www.se.com.

Contact your local Schneider Electric representative to learn what additional training opportunities are available regarding the PowerLogic™ ION7400 series meter.

Make sure you are using the most up-to-date version of your meter’s firmware in order to access the latest features.

Print version

The PDF version of this help can be downloaded from se.com at the following link:

https://www.se.com/ca/en/download/document/7EN02-0374/

Related documents

 
Document Number or link
PowerLogic™ ION7400 online documents

https://www.se.com/ca/en/product-range/63502-powerlogic-ion7400/#documents

PowerLogic™ ION7400 series - MID/MIR installation guide PHA15130
PowerLogic™ ION7400 series - Panel Mount installation guide NHA51491
PowerLogic™ ION7400 series - DIN Mount installation guide NHA77417
ION Reference

ION Reference Help.

Printed version: 7EN02-0290

PowerLogic™ ION7400 series technical datasheet PLSED310113EN