Configuring BACnet/IP using ION Setup
Use ION Setup to configure BACnet/IP.
Prerequisites:
- Firmware version 4.6.0 or later.
 - Communication configuration security access.
 - The BBMD address when using foreign device mode. If you do not know the BBMD address, contact your local network administrator.
 - 
                                                
Read, understand, and implement relevant cybersecurity mitigation strategies outlined in Security risks and mitigation strategies and System defense-in-depth assumptions.
If your BACnet network uses BBMDs, ensure that you understand how to help mitigate risk in your network. BBMDs allow broadcast messages to traverse IP routers.
notice
UNAUTHORIZED ACCESS or network disruption
● Encrypt data over all external connections. ● Physically segment control system networks from non-control system networks. ● Monitor and manage communication loads. Failure to follow these instructions can result in unauthorized or unintended access to data or cause network disruption.
 
There are two steps to configure BACnet/IP:
- 
                                                
Turn on BACnet/IP.
 - 
                                                
Enter your BACnet/IP settings.
 
To turn on BACnet/IP:
- Open ION Setup.
 - Open the Setup Assistant for your meter.
 - Select Communications > Advanced Ethernet > Protocols.
 - 
                                                
Select BACnet/IP, and then select Edit.
If prompted, enter the device credentials.
The BACnet/IP Protocol Settings screen appears.
 - Select Enabled.
 - Select OK to turn on BACnet/IP.
 
To enter your BACnet/IP settings:
- Open the Setup Assistant for your meter.
 - Select Communications > 3rd Party Protocols > BACnet.
 - Enter your BACnet/IP settings.