Configuring serial communications settings using ION Setup
Use ION Setup to configure the meter’s serial communications settings.
Prerequisites:
Make sure you have
a unique unit ID for your meter and know the serial network settings
(protocol, baud rate, parity and stop bits).
To configure the meter’s serial communications settings using ION Setup:
- Start ION Setup.
- Open the Setup Assistant for your
device.
- Click Communications > Serial Settings.
- Select Com1.
- Select a setting, and then click Edit to configure the setting to match your communications system.
Serial communications settings available using ION Setup| Protocol | ION, Modbus RTU,
Modbus Master, DNP v3.00, DLMS, EtherGate, GPS: Truetime/Datum, GPS: Arbiter, GPS: Arbiter-Vorne,
Factory, None | Sets the communications
protocol for your meter’s RS-485 port The NONE setting stops communications using this port. |
| Baud
Rate | 2400,
4800, 9600, 19200, 38400, 57600, 115200 | Sets the data rate,
in bits per second |
| Rx
Timeout1 | 0.1–15 | Sets the transmit
delay (timeout for receiving an entire message from a device) in seconds. |
| Unit
ID | 1–9999 | Sets the meter’s
unique ID on the RS-485 network Note: Modbus serial device range
1 to 247 |
| Serial
Port | 8N1,
8N2, 8E1, 8E2, 8O1, 8O2 | Sets the parity
and stop bits for the port |
| RS485
Bias | OFF,
ON | Turns on biasing
on the client device over the RS-485 port |
1 Only applies to a subset of protocols.