Ethernet Modbus device prerequisites
For your meter to operate as an Ethernet Modbus device, you must complete some prerequisite configuration.
Note: You do not need to perform any Modbus-specific configuration for your meter to function as a Modbus client device over Ethernet.
Prerequisite | Description |
---|---|
Ethernet | All devices must have a working Ethernet connection. |
IP address | All devices must have a unique IP address. |
Port | All devices must be communicating over Ethernet port 502 for Modbus TCP. |
Note: Devices supporting multiple simultaneous Modbus TCP connections can have communications delays. Adjust your network timeout settings to accommodate this.