Simple Network Management Protocol (SNMP)

Your meter supports Simple Network Management Protocol (SNMP) after you have enabled SNMP on your meter. You need to upload the meter’s Management Information Base (MIB) file (available from www.se.com) into the Network Management System (NMS) managing your meter.

SNMP is part of the Transmission Control Protocol/Internet Protocol (TCP/IP) protocol suite. SNMP is an application layer protocol that enables the exchange of network management information between devices, allowing you to manage network performance and to identify and solve problems on networks with devices of various types.

SNMP configuration assumes that you have an advanced understanding of SNMP and the communications network and power system that your meter is connected to.

Key terms

Term Definition

Agent

Software resident on the managed device which interfaces between the device and the NMS.

Managed device

Your meter in the SNMP network.

Community name/string A text string that helps authenticate requests between the managed device and the NMS.
Managed object Any parameter referenced in the MIB file.
MIB A management information base which organizes the OIDs in a hierarchical tree.
NMS A network management station, manager or client that executes applications to monitor and control devices. An NMS must have the standard and custom MIB files and SNMP manager software.
OID An object identifier that uniquely identifies and labels a managed object in the MIB.
Trap receiver An NMS that is configured to receive traps and whose IP address is an SNMP trap destination.