Configuring option module analog outputs using ION Setup
You can configure option module analog outputs using ION Setup.
Analog outputs are available on the optional I/O modules.
Calculate your zero scale and full scale values based on the measured value and the analog output range of your meter.
Make sure that the analog output port that you want to use is properly connected to an analog receiver.
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Click Expansion Modules > Option I/O Modules and select the module tab that corresponds to the option module with the analog output you want to configure.
- Select the analog output channel and click Edit. Enter the meter password if prompted. The setup screen for that analog output is displayed.
- Configure the analog output by selecting the parameter
and clicking Edit.
Parameter Value/Range Description Zero scale 0 to ±109 The minimum source value that matches the minimum analog output signal. Full scale 0 to ±109 The maximum source value that matches the maximum analog output signal. Port - The physical analog output port connection. Mode Voltage, current Determines whether the analog output is monitoring voltage or current.