Voltage crest factor

Crest factor is the ratio of peak to RMS voltage values.

For a pure sinusoidal waveform, crest factor is equal to 1.414. The meter uses the following equation to calculate crest factor:

C = Crest factor

Vpeak = Voltage peak

VRMS = Voltage RMS