Clock source time quality flag
The meter’s clock source time quality flag is primarily used to report time quality information for digital input events, such as status alarms, in Sequence-of-Events Recording (SER) applications.
The meter keeps track of the time difference between the meter’s internal clock and the time sync source.
When the meter’s Clock module’s Use Clock Source Qual Flag is set to use flag, the Diagnostics module’s Receiver Status output register is set to:
- locked if the time difference between the GPS time sync source or PTP leader and meter clock is within ±1 ms of each other
- unlocked if the time difference between the GPS time sync source or PTP leader and meter clock is greater than ±1 ms of each other