Putting your meter in test mode using ION Setup

Prerequisites:

  • To put your meter into test mode, your meter must be:

    1. Revenue-unlocked

      OR

    2. In a pending state (pending lock or pending unlock)

      If you are unsure of the meter revenue-lock state, see Revenue lock LED behavior.

To put your meter into test mode using ION Setup:

  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Navigate to Verification and then select Verification.
  4. Select Test Mode and then select Display.

    Your meter is now in test mode, and the Test Mode screen is displayed.

  5. Select the different tabs to view your meter’s test mode values and modify test mode parameters.
  6. Select Close to exit test mode.