Creating and importing projects using CAE

Conditions préalables :

  • Project Management permission.

There are two ways to add a project in CAE:

  1. Creating a new project.

  2. Importing a project.

Creating a new project

To create a new project:

  1. Select menu icon > Projects.

  2. Select Create Project.

  3. Enter your Project Details.

    Remarque : Select Substation / Feeder Automation for the Architecture.

  4. Select Save.

  5. Open your project.

Importing a project

To import a project:

  1. Select menu icon > Projects.

  2. Select Import Project.

  3. Select Browse and then choose the project that you want to import.

  4. Enter the Password to decrypt the project file.

  5. Select Import.

  6. Open your project.