Templates and firmware

Your meter comes installed with a preconfigured default template. This template contains various frameworks which provide all the power measuring and analyzing functionality of the meter. The default templates and frameworks can be used immediately without any user configuration. They can also be customized, reconfigured, and pasted from one meter to another.

For more information on templates, frameworks and ION modules, see the ION Reference.

Firmware is your meter’s operating system. When newer firmware is available for your meter, simply upgrade to the latest version for all the added features and functionality.

 

Topics in this section: