Basic setup parameters

Menu item Setting options Default Description
Volts mode1
  • 9S - 4 Wire Wye/Delta
  • 29S - 4 Wire Wye
  • 35S - 3 Wire
  • 36S - 4 Wire Wye
  • Demo
*See note

The power system’s configuration and supported form factor. 36S - 4 Wire Wye is only available on the socket meter.

 

Note: The default setting varies depending on the meter form factor. Ensure you verify that the correct option is selected for your power system before putting the meter into service.

PT Primary1 1.0 to 999999.00 120 The Potential Transformer’s primary winding rating
PT Secondary1 1.0 to 999999.00 120 The Potential Transformer’s secondary winding rating
CT Primary1 1.0 to 999999.00 5 The Current Transformer’s primary winding rating
CT Secondary1 1.0 to 999999.00 5 The Current Transformer’s secondary winding rating
VA Polarity
  • normal
  • inverted
NORMAL The polarity of the Potential Transformer on V1
VB Polarity
  • normal
  • inverted
NORMAL The polarity of the Potential Transformer on V2
VC Polarity
  • normal
  • inverted
NORMAL The polarity of the Potential Transformer on V3
IA Polarity
  • normal
  • inverted
NORMAL The polarity of the Current Transformer on I1
IB Polarity
  • normal
  • inverted
NORMAL The polarity of the Current Transformer on I2
IC Polarity
  • normal
  • inverted
NORMAL The polarity of the Current Transformer on I3
Phase Rotation
  • ABC
  • ACB
ABC The expected rotation of the voltage phases (ABC or ACB)
ScaleRevParam
  • ON
  • OFF
ON Whether or not PT/CT correction is applied to displayed and recorded meter data

1 These registers are typically set when the device is commissioned. Changing the values of these registers while the device is in service is not recommended.