Basic setup
This chapter explains how to perform basic meter setup using the front panel, Power Monitoring Expert or ION Setup.
Basic configuration of the meter is provided by the Power Meter module. The Power Meter module is the main connection between the power system measurements and all other ION modules in the device. This module reports the values for all voltage, current and power measurements. The Power Meter module’s setup registers describe details of the power system being monitored.
Basic setup is typically performed when the meter is initially put into service, although the device cannot operate properly until the Volts Mode and PT and CT ratios are set. After this basic setup is performed the meter operates properly, and there is generally no need to make further changes to the basic setup.
Other advanced parameters can be configured, if needed. See the description of the Power Meter module in ION Reference for more information.
Topics in this section: