Overwriting communication module registers

To overwrite the communication module registers: 

  1. Open ION Setup.
  2. Ctrl + click on the meter to select it. This switches ION Setup to Advanced.
  3. Double-click Comm Modules folder > Ethernet > Setup Registers.
  4. Type text or characters to replace values for network infrastructure setup registers by selecting them and clicking Edit. Some registers include:
    • IP Address.
    • IP Mask.
    • IP Gateway.
    • NOTE: IP values can be replaced with text.

    • Primary DNS.
    • Secondary DNS.
    • All servers.
    • All port numbers.
  5. Click Send.