Overwriting factory module registers
To overwrite the factory module register:
- Open ION Setup.
- Ctrl + click on the meter to select it. This switches ION Setup to Advanced mode.
- Double-click Factory Modules folder > select meter type.
- Select the Setup Registers tab.
- Type text or characters to replace values for these setup registers by selecting them and click Edit:
- FAC1 Device Namespace.
- FAC1 Device Name.
- FAC1 Owner.
- FAC1 Tag1.
- FAC1 Tag2.
- Click Send.