Overwriting the meter template file

To overwrite the meter template file: 

  1. Go to www.se.com and search for the meter template for your device.
  2. Download the ZIP file and extract files.
  3. Open ION Setup.
  4. Click the meter to select it > Setup Assistant.
  5. Template > Send to Meter tab.
  6. Click Send.
  7. Navigate to the extracted files and select the DCF file.
  8. NOTE: FWN file type is also an option.

  9. Click Open.
  10. Click Proceed. The Template Paste Options dialog box opens.
  11. Clear all check boxes and click OK.
  12. Click Yes. The overwriting process could take a few minutes.
  13. Click OK.
  14. Click Exit and then OK.