Passwords

Recommendations to optimize cybersecurity in a protected environment:

  • Document and store passwords and usernames in a protected location.
  • notice

    data Loss

    Record your device's front panel and user password information in a secure location.

    Failure to follow these instructions can result in data loss.

     

  • Change the default password of 0 (zero) to help reduce unauthorized access.
  • Default account settings are often the source of unauthorized access by malicious users.

  • View the Device Configuration Checklist to quickly determine if the default password is used:
  • Use Advanced security mode.
  • Use alphanumeric passwords with a length of six characters.
  • Follow user account management tasks as described by your organization or contact your Network Administrator, for example, maximum password age or history policies.