Updating passwords on multiple meters

Use the ION Setup Diagnostics tool to update passwords on multiple meters at the same time.

Required for this procedure:

  • Meter connection using ION Setup.
  • Login credentials.
  • Security configuration access privileges.

notice

LOSS of DATA

Record your device's user and password information in a secure location.

Failure to follow these instructions can result in equipment damage.

 

To update passwords on multiple meters:

  1. Open ION Setup > select the System.
  2. Tools > Diagnostics. The Systems diagnostics: System dialog box opens.
  3. Select the Tools tab > Advanced Security Password Updater.
  4. Click Open.
  5. Select the meters that need a password update.
  6. Click Set Info.
  7. Click Start.
  8. Click Allow passwords to be visible.
  9. Select each user, click Password and enter a new password.
  10. If the meter is connected to a display, update the password for the Front Panel.

  11. Click Start. A Notice message box opens.
  12. Click Proceed. A result is displayed for each device.
  13. Click Save As to save a copy of updated meter passwords in a .txt file. The Save As dialog box opens.
  14. Save the file with a unique file name to a protected location. An ION Setup message box opens.
  15. Click OK.
  16. Click Exit.
  17. Click Close.