Third party protocols
This
It also contains brief instructions for configuring your meter to work with MV-90 systems.
For additional instructions on using the meter with Modbus, DLMS, IRIG-B, IEC 61850 and MV-90 protocols, see the following documents:
- Modbus protocol and register map for ION devices protocol document
- Modbus and ION Technology technical note
- DLMS/COSEM and ION technology protocol document
- IRIG-B GPS Time Synchronization technical note
- IEC 61850 and ION technology protocol document
- MV90 and ION technology technical note
Topics in this section: