Event logging
Events produced by the meter’s various ION modules are prioritized and grouped to facilitate custom logging. Each event is assigned a priority group number based on its type and severity.
Event priority groups
Some event groups are preset with a priority number as shown in the table below. You can also define your own priority number for some modules. Priority numbers from 128- 191 appear in the global event log viewer in the Vista component of Power Monitoring Expert. Priority numbers from 192-255 are also logged, initiate a beep and cause the window to flash. You can customize these responses to display messages or perform netsend messages, for example.
|
Event group |
Description |
Priority number |
|
Reset |
Module reset or re-synchronized |
5 |
|
Setup Change |
Module setup changes (setup register changes, label changes, input handle changes) |
10 |
|
Input Register Change |
Inputs of certain modules change value (for example, input to And/Or module changes) |
15 |
|
I/O State Change |
I/O state changes (for example, relay closes) |
20 |
|
Information |
Module produces important user information |
25 |
|
Warning |
Module produces a warning |
30 |
|
EN50160 Event (ION8650A and ION8650B only) |
An EN50160 counter (N1or N2) increases |
50 |
|
Loss of Potential |
Loss of Potential has occurred |
128 |
|
Error Detected |
An error has been detected |
255 |
|
Setpoint |
Setpoint condition goes Active or Inactive (for example, Sag/Swell module detects a disturbance) |
programmable via module setup |
The Event Log Controller module allows you to set a priority cutoff for event logging. Any events with a priority number greater than the cutoff value are logged, and events with lower priorities are discarded. Refer to the individual module descriptions and the Event Log Controller module description in the ION Reference for more details.
Events external to the module
Some events are not produced by a specific module. These events are generated internally by the meter. Their associated priority levels are shown in the table below.
|
Event group |
Description |
Priority number |
|
Warning |
Factory initialize performed |
30 |
|
Firmware or memory upgrade performed |
||
|
Meter power-up or power-down |
||
|
Internal modem not responding or modem recovered |
||
|
Battery low |
||
|
Serial terminal locked out |
||
|
Security disabled or enabled |
||
|
Failure |
Communications not able to allocate required memory |
255 |
User triggered events
When a user produces an event, such as a reset, successful or unsuccessful login attempts, user lockout or setup change, the event log displays the username associated with the event. Events created in basic security through the front panel have the username USER0. Events created in advanced security through the front panel or ION Setup are associated with the username that was logged into the meter (USER1 - USER50).
Displaying events
View events in the following locations:
|
Application |
Menu / screen |
Navigation |
|
Front Panel |
Event Log |
ALT display mode |
|
ION Setup |
Event Log |
Setup Assistant > Reports > Event Log |
|
Vista |
Meter Events |
Volts/Amps tab > Meter events object |