Displays

The meter ships with preconfigured front panel display screens designed to suit the data needs of most users. Different types of screens are available depending on the meter’s current mode of operation (see Modes of operation for details).

Front panel displays can also be customized on your meter to show virtually any measurement or calculation. For example, you can:

  • Change displayed parameters, such as from Vll to Vln or Vllab to Vlna
  • Adjust character size to be different on each screen
  • Change data display settings such as backlight timeout, automatic display scrolling, parameter update rate, display mode and display units.

This section explains the available front panel displays. It also includes procedures for customizing displays using Power Monitoring Expert or ION Setup.

 

Topics in this section: